Renesas Synergy™

FAQ 1000178 : WindowsXPのパソコンを、SP2からSP3にアップデートしても、使用に問題はないか?

Q : 質問

WindowsXPのパソコンを、Service Pack2からService Pack3にアップデートしても、スタータキットの使用に問題はないか?

 


A:回答

WindowsXP(SP3)でのご使用ですが、SP3は主にセキュリティ改善であり、一般のユーザには影響のない部分の変更と認識しております。 このため、Windows XP Service Pack2への対応に準じますので、スタータキット付属のツールで使用いただいても問題ございません。

 

 

適用製品

Renesas Starter Kit for M16C/26A
Renesas Starter Kit for M16C/29
Renesas Starter Kit for M16C/62P
Renesas Starter Kit for M32C/87
Renesas Starter Kit for R8C/25
Renesas Starter Kit for M16C/6NK
Renesas Starter Kit for H8/38347
Renesas Starter Kit for R8C/27
Renesas Starter Kit for R8C/23
Renesas Starter Kit for R8C/2D
Renesas Starter Kit for H8/38099
Renesas Starter Kit for H8/36079
Renesas Starter Kit for 38D5
Renesas Starter Kit for R32C/111
Renesas Starter Kit for R32C/118
Renesas Starter Kit for M16C/65
Renesas Starter Kit for RX610
Renesas Starter Kit for R8C/L3AC
Renesas Starter Kit for R8C/35C
Renesas Starter Kit for R8C/38C
Renesas Starter Kit+ for RX62N
Renesas Starter Kit for R8C/LA8A
Renesas Starter Kit for RL78/G13
Renesas Starter Kit for RX210
Renesas Starter Kit for RL78/G14
Renesas Starter Kit for RX630
Renesas Starter Kit+ for RX63N
Renesas Starter Kit for RX62G

 

他にご質問がございましたら、リクエストを送信してください